2410_LSS100100/LSS100200_SW_03.0

Security Recommendations

To enhance the security of your controller, consider the following best practices:

  1. Network security:

    • Set up network security at an appropriate level.

    • Ensure that your controller is part of a secure network with limited access.

    • If connected to the Internet, strictly recommend using either a VPN or an HTTPS communication.

  2. Secure protocol access:

    • Use the secure protocol HTTPS://IP:Port to access your controller.

  3. Security measures:

    • Evaluate the security capabilities of other network elements, such as firewalls and protection against viruses and malware threats.

    • Store backup files in a safe location inaccessible to unauthorized individuals.

  4. Public IP address:

    • Verify that your controller does not have a publicly accessible IP address.

    • Avoid using port forwarding to access your controller from the public Internet.

  5. Network segmentation:

    • Place your controller on its own network segment.

    • If your router supports a guest network or VLAN, consider locating controller there.

  6. Cybersecurity incidents and vulnerabilities:

  7. HTTP communication warning:

    • If HTTP communication is detected, switch to HTTPS (encrypted mode).

    • Note that your controller comes with a self-signed SSL certificate, which encrypts information. Web browsers may display a warning message when confirming the exception to proceed.

  8. KNX installation security:

    • When accessing the KNX installation via the Internet, be aware that data traffic can be read by third parties.

    • Always use a VPN connection with secure encryption for all data packets.

    • Hardware requirements for VPN routers and features offered by mobile service providers may vary significantly.

For additional details on system hardening, refer to Schneider Electric’s document: System Hardening Guidelines for Wiser for KNX and spaceLYnk Controllers.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?