250929_LSS100100/LSS100200_SW_03.0

Add New User

To add a new user, follow these steps:

  1. Open the User access tab.

  2. Click the Add new user button located at the bottom left corner.

  3. Update the user access settings as needed.

Here are the details for each field in the General section of the User dialog:

  • Name: Enter the name of the account.

  • Login: Use a login name with a length between 2 and 20 characters. Accepted characters include “-”, “_”, lowercase letters (a-z), and digits (0-9).

  • Active: Activate or deactivate the user account.

  • Password: Set a password with a length at least 8 characters. Password must contain at least one uppercase letter, lowercase letter, and a digit..

Next, configure access levels for the user:

  • Visualization/Schedulers/Trends access:

    • Choose from NonePartial, or Full access. If you select partial access, the Visualization, Schedulers, and Trend logs tabs become active, allowing you to specify parameters.

  • Touch access:

    • Select either Partial or Full access. If you select partial access, the Touch tab becomes active, allowing you to specify which rooms are visible in the Touch visualization. Check the rooms the user is allowed to access..

  • Homepage: Set the page the user sees after logging in (e.g., default Start page or a specific application).

  • Applications access: If you choose partial access in the General tab, the Applications tab becomes active. Select the applications the user can access from the Start page.

  • Advanced: Provide a list of group addresses available to users.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?