250929_LSS100100/LSS100200_SW_03.0

Default Configuration

If the default password has not been changed, you will be prompted to enter the admin access password. This applies to brand new controllers or after a firmware upgrade.


Password complexity requirements:

  • The password must be 8-20 characters long.

  • It should contain uppercase letters from European languages (A through Z, including diacritic marks, Greek, and Cyrillic characters).

  • It must also include lowercase letters from European languages (a through z, including sharp-s, diacritic marks, Greek, and Cyrillic characters).

  • Additionally, the password should have at least one base 10 digit (0 through 9).


LAN configuration:

  • IP Address on LAN: 192.168.0.10

  • Network Mask on LAN: 255.255.255.0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?