250929_LSS100100/LSS100200_SW_03.0

Backup Configuration

If you wish to create a backup of your configuration, do the following:

  1. Navigate to SystemBackup configuration.

  2. Choose your password, confirm it by re-entering, and then click OK.

The controller will backup the system configuration and generate a backup file.

See also Backup.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?