250929_LSS100100/LSS100200_SW_03.0

Structure

To navigate between plans, layouts, and structure widgets, use the navigation tree in the structured view.

In editing mode, the following additional parameters are available:

  • Size of plans, layouts, or widgets

  • Source picture/background color

Ensure that the plan size is correctly positioned against the background. Widget size should always be smaller than the plan it is placed on. Use component positioning to align objects.

Click the Vis.configuration button to adjust visualization parameters according to your needs.

To reorder objects in smartphone visualization, click .

Next to the Reorder smartphone objects icon, you will find two icons for quick access:

  • Preview in PC/tablet

  • Preview in smartphone

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?