250929_LSS100100/LSS100200_SW_03.0

Image

The Image tab allows you to add images to the visualization map either from local storage or the internet. External images are particularly useful for dynamic weathercast visuals. To configure your image, follow these steps:

  1. Image source:

    • Choose either Local or Remote as the image source.

    • If using a remote image, provide the URL.

  2. Select image:

    • Pick an image that you have previously added to the Vis. graphicsImages/Backgrounds section.

  3. Image size:

    • Specify the desired dimensions for your image.

  4. External link:

    • Define an external link URL that users can access by clicking the image (e.g., http://www.se.com).

  5. Refresh interval:

    • Set the interval for refreshing the image when it is sourced externally.

  6. Additional classes:

    • Creates custom CSS classes to modify graphical objects.

Once you have configured the image parameters, click the Add to plan button. A new object will appear on the map, which you can move to your desired location. If necessary, resize the image by grabbing its edges.

Remember to adjust the element size and position (refer to Object).

Finally, click Save and reload plan to apply your changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?