250929_LSS100100/LSS100200_SW_03.0

User Roles and Permissions

  1. Administrator (Admin):

    • Unrestricted access to all tabs and settings in the controller.

    • Responsible for granting and revoking access for other users.

    • Sets restrictions on user access.

    NOTE: The administrator cannot grant access to the Configuration tab, which includes critical settings like system settings and KNX management.

  2. Users: Users can access various tabs and settings based on the administrator's restrictions. They may have full or partial access to the following:

    • Visualization: Access to view a property visualization.

    • Scheduler: Access to view and edit schedulers.

    • Trends: Access to view stored data trends.

    • Applications: Access to view and configure some installed applications.

    • Touch: Access to rooms in the control panel.


When the Management plugin is installed, users may have access to the following settings, depending on administrator restrictions:

  • Device sharing: Ability to grant access to another user account for the controller in the mobile application.

  • Controller API: Ability to enable or disable the REST API.

  • Cloud access: Ability to log out/into the cloud, unpair a controller, or delete a homeowner account.

  • Modbus profiles: Access to the Modbus profiles library.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?