250929_LSS100100/LSS100200_SW_03.0

Start Page

The start page offers a dashboard-like view, highlighting key areas within your controller. Here are the available options:

  1. User name and password setup:

    • Upon the first login or after a factory reset, you’ll be prompted to set your user name and password.

    • The default Admin login credentials are as follows:

      • User name: admin

      • Password: admin

    • Note that initially, only an Admin account exists. Additional users must be created. Refer to chapter User Access for details on user access.

  2. PC/Tablet:

    • Click this icon to access a rich visualization interface with plans containing individual objects.

    • Ideal for use on PCs, iPads, and Android tablets (preferably with a display size of 10 inches or larger).

  3. Smartphone:

    • This icon leads to a simplified list visualization designed for iPhone/iPad/Android smartphones and Android tablets (with a display size of 7 inches or smaller).

    • All objects added in controller visualization are visible here (unless the Hide in Smartphone option is enabled). Different icons may be set for smartphone visualization.

  4. Scheduler:

    • Navigate to a user-friendly interface for managing scheduler tasks.

  5. Trends:

    • Access a user-friendly display of Trend logs, allowing you to compare values over time.

    • Trends can be displayed for up to 10 years.

  6. Touch:

    • Explore the visualization created in the Touch Config environment.

  7. Touch Config:

    • This icon takes you to the premade widgets visualization creator.

  8. Configurator:

    • Navigate to the programming, settings, and configuration interface.

    • Access is restricted to administrators.

    • Using the Configurator on mobile devices is not recommended.

  9. Function Blocks Editor:

    • Click this icon to access the FB Editor, which provides a graphical and user-friendly alternative to LUA scripting.

  10. KNX IoT 3rd Party API:

    • Serves as an interface for third-party applications to interact with KNX systems. Enables communication between external software and KNX devices, allowing developers to create custom integrations, applications, or services.

    • Enable the API for cloud and/or local integration.

    • For KNX IoT 3rd Party API documentation, please reach out to the customer care support team.

  11. KNX IoT 3rd Party API Config

  12. Cloud connector:

    • Establish a connection to the KNX cloud.

NOTE: Firmware (Upgrade Firmware) automatically installs the Cloud connectorKNX IoT 3rd Party API, and Touch visualization applications in the controller together with a new feature that allows the automatic update of the applications. It is highly recommended that you enable automatic updates. Then you do not have to manually update the applications in the controller´s Marketplace in the future.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.