2410_LSS100100/LSS100200_SW_03.0

ETS 3

To utilize controller with KNX TP UART/IP functionality and program other KNX bus devices, follow these steps to add your controller to the ETS Connection manager.

ETS programming through the controller is available only when KNX IP features are enabled.

NOTE: The function Bus monitor is not included in the controller.

  1. Navigate to Extras > Options > Communication > Configure Interfaces.

  2. Enter a name for the connection.

  3. Choose the Type and select KNXnet/IP from the drop-down menu.

  4. Click Rescan and then select spaceLYnk/ Wiser for KNX  from the drop-down menu.

  5. Click OK.

  6. In the Options > Communication window, select the newly created interface as the Communication interface from the drop-down menu.

  7. To test communication with ETS, click Test.

  8. Ensure that the bus status is Online by clicking in ETS.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?