250929_LSS100100/LSS100200_SW_03.0

Adding Widgets

To add a new widget, follow these steps:

  1. Open the room you want to add the widget to in Touch Config.

  2. Click the + button at the top right of the screen.

  3. The Add new widget menu will open. Select the widget you want to place in the room.

  4. A widget dialog will appear, allowing you to set a widget name, assign objects to your widget, and choose a display style for your widget.

  5. Ensure that all required objects are linked for the widget to appear correctly in the visualization structure.

    NOTE: Objects marked with an asterisk (*) are mandatory. Additionally, some objects include an alert field. Fill in this field, and the object will generate an alert when the alarm condition is met.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?