250929_LSS100100/LSS100200_SW_03.0

Add Scheduler

To create a new scheduler, follow these steps:

  1. Click the Add Scheduler button at the bottom left.

  2. Fill in the Scheduler dialog with the following details:

    • Object: Specify the group address that the scheduler will control.

    • Active: Define whether the scheduler is active or not.

    • Scheduler On/Off object: Choose an object that can enable or disable the scheduler.

    • Name: Provide a name for the scheduler.

    • Category: Sort schedulers into created categories for better clarity.

    • Start date: Set the start date for the scheduler.

    • End date: Specify the end date for the scheduler.

  3. Click Save.

Your scheduler will now appear in the Schedulers list, where you can edit or delete it as needed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?