250929_LSS100100/LSS100200_SW_03.0

Visualization Parameters

To configure the visualization parameters for a specific object, follow these steps:

  1. Click corresponding to your object.

  2. Adjust the visualization parameters as needed.

  3. Click Save.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?