250929_LSS100100/LSS100200_SW_03.0

Restore Configuration

If you wish to restore your system configuration from a backup file, do the following:

  1. Navigate to SystemRestore configuration.

  2. Choose your backup file, enter your password, and then click OK.

The controller reboots automatically after configuration has been restored.

See also: Restore.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?