250929_LSS100100/LSS100200_SW_03.0

HTTP SSL Certificate

SSL certificates are small data files that digitally link a cryptographic key to a device’s details. When installed on a web server, it activates the padlock and the HTTPS protocol, allowing secure connections from a web server to a browser.


There are numerous online SSL certificate providers, offering both free and paid options.

Mode:

  • Upload new private key/certificate: This mode is for uploading an existing RSA key or SSL certificate.

  • Generate new private key/certificate: This mode allows you to generate a new RSA private key or SSL certificate from one that is already installed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?