250929_LSS100100/LSS100200_SW_03.0

Object Control Bar

The object control bar at the bottom of the Objects tab includes the following buttons and information:

  1. Add new object: Manually add new objects to the list.

  2. Auto update enabled: Specifies whether the object list is updated automatically or not.

  3. Clear: Clears the list of filtered group addresses.

  4. Mass edit: Allows mass editing of selected filter objects. See example in Object Filter.

  5. Mass delete: Enables mass deletion of selected objects. See example in .

  6. Next/Previous page: Navigate to the next or previous page.

  7. Refresh: Refreshes the object list.

  8. IP > Loc policy: Displays the selected filtering policy.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?