250929_LSS100100/LSS100200_SW_03.0

Event-Based Script

Event-based scripts execute when a group event occurs on the bus. They are particularly useful for real-time responses. To create an event-based script, follow these steps:

  1. Click Event-based button in the Scripting tab → click the Add new script button.

  2. Set the parameters in the Event-based script dialog as follows:

    • Script name: Provide a descriptive name for the script.

    • Group address/tag:

      • Manually enter group addresses (using digits from 0 to 15) or select from the drop-down list.

      • Group address format: Use digits and “/” as a separator (e.g., 1/1/1).

      • If tags are attached to group addresses, the script can run based on those tags.

    • Active: Set the script’s activation status (green for active, red for disabled).

    • Execute on group read: Choose whether to run the script with every group read.

    • Execution mode:

      • Normal: The event script runs each time it’s triggered.

      • First instance only: Does not start a new script (PID) if it’s already running.

      • Last instance only: Stops all running scripts and PIDs, executing only the last one triggered. Commonly used when saving the current PID into storage.

    • Category: Assign the script to a new or existing category. This helps organize scripts in the Print script listings page under Tools.

    • Description: Add a brief description of the script.

If the script runs only on a read request, consider using the following example:

if event.type == 'groupread' then
-- Your script logic here
end

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?