250929_LSS100100/LSS100200_SW_03.0

Getting Started

Follow these steps to set up your controller:

  1. Mounting:

    • Securely mount the controller on the DIN rail.

  2. Cable connections:

    • Connect the necessary bus cables, including KNX, Modbus, and/or RS232.

    • Optionally, connect a flash drive.

  3. Power supply:

    • Connect a 24V power supply to the device.

    • Ensure the positive conductor is connected to the red clamp, and the negative conductor to the blue clamp.

    • Consider using the recommended accessory: Power supply REG/24V DC/0.4A (article No.: MTN693003).

  4. Ethernet connection:

    • Connect an Ethernet cable from your PC to the controller.

  5. IP address configuration:

    • The default IP address for the controller is 192.168.0.10.

    • Adjust your computer’s IP address to be in the same range, e.g., 192.168.0.9 with a subnet mask of 255.255.255.0.

  6. Web browser access:

    • Open Google Chrome or Mozilla Firefox (for Windows), or Safari (for macOS).

    • Navigate to 192.168.0.10.

  7. Default login credentials:

    • User name: admin

    • Password: admin

Upon login, you will be prompted to change your password. Refer to chapter Default Configuration for details on default configuration settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.