250929_LSS100100/LSS100200_SW_03.0

Reset/Clean-up

This function allows you to delete selected items from the controller.

If you choose to delete objects, they will also be removed from the visualization section.

IMPORTANT: Please ensure that you have backed up all important data before proceeding with the Reset/Clean-Up function.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?