Plans
A plan can represent either a single room within a flat, combining various functions, or a specific function (such as lighting or heating) for the entire flat.
To add plans, follow these steps:
-
Click the
button next to the desired level under
which the plan should be added. -
Select Add plan.
-
Fill in the Plan dialog with the following details:
-
Name: Provide a name for the plan.
-
Plan size: Choose the size of the plan (pre-defined sizes are available in the drop-down menu).
-
Layout: Specify the layout for this plan. Objects from the layout will be duplicated on this particular plan, including background color and the plan image. Ensure that the layout is defined before adding the plan.
-
PC/Tablet visualization: Set visibility for this plan in PC/Tablet visualization.
-
Smartphone visualization: Set visibility for this plan in Smartphone visualization.
-
Pin code: Optionally protect each plan with a PIN code (minimum 4 digits with brute force protection).
-
Primary background image: Select the primary background for the plan.
-
Secondary background image: Choose the secondary background for a parallax effect. Use a background previously added to Vis. graphics → Images/Backgrounds.
-
Background color: Pick the background color for the plan.
-
Smartphone background color: Choose the background color for smartphone visualization.
-
Repeat background image: Decide whether to show the image once or repeat it to fill the entire plan.
-
Fixed primary background: Use a static primary picture for Parallax projection.
-
-
Click Save.
Your new plan will appear in the Levels/Plans tab under the respective level. You can further edit it, duplicate it along with all its components, change its sort order, or delete it.