250929_LSS100100/LSS100200_SW_03.0

Install Updates

Click the Install updates button to apply partial updates or patches, or to add pre-made solutions.

To update Wiser for KNX, install the update file with the *.lmup extension.

NOTE: Wiser for KNX will reboot after a successful update.

Package file signature:

It is important to note that updates installed from the file are verified by a signature. Updates cannot be installed without the correct signature for security reasons. This ensures the integrity and authenticity of the updates.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?