250929_LSS100100/LSS100200_SW_03.0

HTTP Server

The HTTP server allows the use of additional ports for both HTTP and HTTPS.


The default ports are as follows:

  • HTTP Port: 80

  • HTTPS Port: 443


Available HTTPS modes:

  • HTTP and HTTPS enabled

  • HTTPS only, redirect HTTP to HTTPS

  • HTTPS only, HTTP port is disabled


CORS Origin (1 – 4): You can specify up to four IP addresses or hosts that are permitted to use Cross-Origin Resource Sharing (CORS).

IMPORTANT: A system reboot may be required for these changes to take effect.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?