250929_LSS100100/LSS100200_SW_03.0

RTU Scan

The RTU scan feature automatically detects and adds Modbus devices connected to Modbus RTU.

To initiate the scan, click the RTU scan button in the Modbus tab.

Only devices with valid profiles will be added. This feature does not function with custom-made profiles.

For a list of devices supporting automatic discovery, refer to Profiles.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?