250929_LSS100100/LSS100200_SW_03.0

FTP Server

The controller FTP server can be accessed by enabling the FTP server under the Service menu.


Free space: This indicates the remaining free space on the built-in USB card.

Server status: This refers to the current status of the FTP server.

Require encryption (FTPS): When FTP encryption is enabled, the FTP server will only accept secure connections. If it’s not required, the FTP server will accept both FTP and FTPS connections.

Port: This is the port used by the service.

Username: This is the login name (default is ‘ftp’ and ‘apps’ for use with SE services).

Password: This is the password, which should be between 6 and 20 characters. The default password is empty and must be changed before using FTP.

External IP: This is the IP address used for external connections.

Passive mode min/max port: These are the minimum and maximum ports for passive mode.

NOTE: The maximum number of simultaneous FTP connections is limited to 5.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?