250929_LSS100100/LSS100200_SW_03.0

General Configuration

  1. Interface language: Choose from a variety of languages including English, Bulgarian, Chinese, Czech, Danish, Dutch, French, German, Greek, Hungarian, Italian, Polish, Portuguese, Russian, Spanish, Swedish, and Turkish.

  2. Automatic address range start: Define the address range for new group objects.

  3. Virtual address range start: Set the address range for new virtual group objects.

  4. Discover new objects: Enable the KNX object sniffer to automatically add new objects to the objects list. The bus sniffer is enabled by default, but it’s recommended to disable it when not in use, especially if multiple spaceLYnk/Wiser for KNX controllers are connected in the same network.

  5. Object log size: This displays the count of object logs. The maximum limit is 50.000.

  6. Default log policy: Select the log status for all objects or only for checked objects.

  7. Alert log size: This informs you about the count of logged alerts. The maximum limit is 5.000.

  8. Log size: This provides information about the count of logs. The maximum limit is 5.000.

  9. Error log size: This displays the count of logged errors. The maximum limit is 5.000.

  10. Save object values in storage: The script storage is logged and updated when an object value changes.

  11. Code editor tab size: Pressing TAB in the scripting editor inserts a defined number of spaces.

  12. Block unsafe functions in scripts: Enable this option to block potentially harmful functions such as os.exec, io.writefile, etc.

NOTE: The controller maintains the log objects above the limit for 10 minutes. After this period, all records above the limit are cleared. Excessive object logging can degrade the controller performance.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.