250929_LSS100100/LSS100200_SW_03.0

Levels

To add a new level, click Add new level in the Levels/Plans tab.

The main level typically corresponds to the project name. Additional levels can be added later.


For importing a level, click Import → select your level file → click Save.

NOTE: Plans and visualization structures can be imported from another project, with the option to retain or clear linked objects.


The Change sort order button opens a window for drag-and-drop ordering within the visualization structure.

Second level: The second level is utilized in buildings with multiple floors. To create an additional level, click button next to the main level. Provide a name and sort order for the new level.

Duplicate level: Each level can be duplicated along with sublevels and plans by clicking next to the level.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?