250929_LSS100100/LSS100200_SW_03.0

802.1X EAP–TLS

EAP-TLS (Extensible Authentication Protocol – Transport Layer Security) authentication is more secure and efficient than credential-based authentication. It automatically occurs without user involvement.

When the controller is within range of the secure network, it initiates and completes the connection autonomously.

To configure EAP-TLS, follow these steps:

  1. Navigate to ConfiguratorSystemServices802.1X EAP–TLS.

  2. Enable the Service status.

  3. Fill in the parameters (provided by a network administrator).

  4. Click OK.

Once configured, your controller can securely connect to an EAP-secured network. This feature is not supported for HW1.xx devices.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?