250929_LSS100100/LSS100200_SW_03.0

IP > Local Filter

This filter either accepts or rejects received telegrams from the defined KNX devices or physical addresses. Please note that all outgoing telegrams are not subjected to this filter.


Apply filter to tunneling: This filter, designed to offer enhanced functionality compared to a standard KNX router, can be applied to the tunneling mode. By default, it allows all telegrams to pass. This option applies to both directions (IP > Local Filter & Local > IP Filter).

SRC policy: This is the policy applied to the list of source addresses. The options include:

  • No filter

  • Accept selected individual addresses

  • Reject selected individual addresses

Individual address list: This list contains the individual or group addresses (one address per line). Use an asterisk (e.g., 1.1.* or 1/1/*) to filter all the addresses in the given line.

DST group policy: This is the policy applied to the list of destination group addresses. The destination group filter either accepts or rejects received telegrams belonging to one group (e.g., 1/2/3) or subgroup (e.g., 1/2/*). All outgoing telegrams are not subjected to this filter. The options include:

  • No filter

  • Accept selected individual addresses

  • Reject selected individual addresses

Group address list: This list contains the group addresses (one address per line). Use an asterisk (e.g., 1/1/*) to filter all the addresses in the given line.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?