250929_LSS100100/LSS100200_SW_03.0

RTU Settings

To communicate with Modbus extensions connected via Modbus RTU (serial), follow these steps:

  1. Click the RTU settings button in the Modbus tab.

  2. Configure the parameters in the RTU settings tab as follows:

    • RTU (serial) enabled:

      • Enable Modbus RTU communication.

      NOTE: Only RTU1 can be set for Modbus communication.
    • Port:

      • Set the name of the serial port.

      • The default setting is /dev/RS485.

    • Parity:

      • Specify the parity or stop bits.

    • Duplex:

      • Choose either Half-duplex or Full-duplex.

      • The default value is Half-duplex.

    • Reset to defaults:

      • Click this button to reset all RTU settings parameters to their default values.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?