250929_LSS100100/LSS100200_SW_03.0

Launching Visualization on iPhone

  1. Ensure that your iPhone is wirelessly connected to the controller via a separate access point (such as a wireless router).

  2. Open your iPhone web browser (Safari).

  3. Enter the controller IP address (default: 192.168.0.10) in the browser.

  4. Click on the Start page of your controller.

  5. To create a shortcut for easy access, save the application link to your iPhone Home screen: Tap in the Safari browser and tap Add to Home Screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?