250929_LSS100100/LSS100200_SW_03.0

Visualization

This Visualization window is divided into three sections:

  1. Structure: This section contains a navigation tree for levels, plans, and widgets that were created under the visualization structure tab.

  2. Visualization map: The actual visualization field where you can add all visualization components.

  3. Plan editor: In this section, you can configure all parameters of the component.

Additionally, both sidebars can be minimized by clicking , which enhances visibility – especially on small displays.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?