250929_LSS100100/LSS100200_SW_03.0

NTP/Client/Server

Client status: Upon enabling the client status, the controller fetches data from a maximum of four selected servers.

Network time protocol (clock synchronization) – Servers 1 – 4: Specify the server from which the controller should retrieve the date and time.

Local server status: By enabling this option, the controller can function as a local NTP server for other devices in the network.


IMPORTANT: A system reboot may be required for changes to take effect. If necessary, use the ping tool to verify the availability of the NTP server.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?