250929_LSS100100/LSS100200_SW_03.0

Trend Log Visualization

You can access trend log visualization by clicking Trends from the Start page of your controller. There, you can choose how to display your trends based on the time period (current or previous), whether to show single or multiple trends, and whether to display them as graphs or raw data.

Additionally, you have the option to export trends in CSV format for further analysis.

Multiple trends export: Exporting multiple trends is supported. However, keep in mind that the total number of trends is flexible and depends on the system memory capacity. Each trend reserves a portion of system memory based on its settings. If the memory becomes full, the system will prevent you from creating additional trends.

To optimize memory usage:

  • Avoid storing data for unnecessarily long periods.

  • Use an appropriate trend sampling rate.

  • Regularly export your trend data.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?