250929_LSS100100/LSS100200_SW_03.0

Application Example

Requirements:

  1. Measure and visualize the energy used for lighting in an office building.

  2. Monitor gas and water consumption within the building.

  3. Ensure operational safety of IT equipment by monitoring network quality.

Solution:

  1. Install an iEM3150 meter to measure energy consumption by the lights.

  2. Use an iEM3255 meter to assess power mains quality.

  3. Employ a SIM10M module with pulse meters to measure gas and water consumption.

  4. Connect all devices via Modbus for seamless communication.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?