250929_LSS100100/LSS100200_SW_03.0

Discover Your Controller in IP Network

  1. Windows OS:

    • Download the utility service browser Bonjour from here.

    • If the host is unchanged and there’s only one controller on the network, type the following in your browser:
      http://spaceLYnk.local
      http://Wiser_for_KNX.local

    NOTE: The installed Bonjour service is required for this functionality.
  2. Linux OS:

    • You can download the utility called Avahi from here.

  3. Android:

    • Download the freely available app called ZeroConf Browser from Google Play.

  4. iOS/Mac OS:

    • You can download the freely available app Discovery DNS-SD Browser from the iOS App Store.

    • For iPad, install the iPhone/iPod version of the utility.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?