250929_LSS100100/LSS100200_SW_03.0

Link

To enhance visualization convenience, plan links have been integrated. These special icons on the map serve as links to other plans.

Follow these steps to set up a link within the Link tab:

  1. Link to:

    • Select the plan link you want to associate with this icon.

  2. Custom name:

    • Type a name for the link.

  3. Hide in Smartphone:

    • Choose whether to display this plan link on smartphones.

  4. Hide background:

    • Toggle the icon background visibility.

  5. Display mode [Icon; Value]:

    • Decide how the plan link should appear.

  6. Icon:

    • Select the icon to display in the visualization. If only text is chosen, text parameters apply.

  7. Active state icon:

    • If an icon is selected, the active plan icon becomes available.

  8. Additional classes:

    • Create custom classes for modifying specific groups of graphical objects using CSS.

After defining these parameters, click Add to plan to create a new link. The Cancel button resets link parameters to default settings.

Links can be moved within the plan, duplicated, and edited.

Element position:

  • Manually add elements or drag and drop elements to set their X and Y axis positions on the plan.

Element size:

  • Adjust the element size manually or by dragging a vertical-horizontal strip of the link.

  • The minimum size value is 5 × 5 pixels.

  • To reset an element size to the default, click .

  • Lock the aspect ratio of the link by clicking .

When you are ready, click Save and reload plan to activate the links.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?