250929_LSS100100/LSS100200_SW_03.0

HomeKit Plugin Installation

  1. Log in to the controller through your web browser.

  2. Click on in the top right corner to open the Marketplace.

  3. Click on the green bar in the middle to display the applications available for installation under Install new apps and widgets

    .
  4. From the list of available applications, select the HomeKit plugin and click on the right to start the installation.

  5. Return to the Start page of your controller in the web browser. The installed HomeKit plugin will appear among other applications:

  6. Click on the HomeKit icon to open the plugin:

NOTE: We recommend enabling the plugin's automatic update to ensure you always have the latest version.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?