250929_LSS100100/LSS100200_SW_03.0

USB

  • Devices complying with the USB specification can consume a total of 500 mA from the bus. This allows devices with a power requirement of up to 2.5 W to be supplied via the bus.

  • Integrated voltage supply (5 VDC) is available for devices connected via the 4-pole USB cable.
  • USB cables must not exceed a maximum length of 4.5 meters according to the specification.

  • Data transmission is possible in both directions.

  • The USB interface is commonly used for extending memory capacity by connecting USB flash drives to computers or other devices.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?