250929_LSS100100/LSS100200_SW_03.0

Script Editor

When you add a script, an icon appears in the Editor column, allowing you to open the script in the script editor. Here are some key features:

  1. Helpers: Save time by using built-in code snippets. Click the appropriate snippet, and it will automatically add code to the editor field.

  2. Keyboard shortcuts:

    • Ctrl + F: Find syntax in your code (text will be highlighted in yellow).

    • Ctrl + G: After finding text via Ctrl + F, use Ctrl + G to select the next syntax in the script.

    • Shift + Ctrl + G: Select the previous syntax.

    • Shift + Ctrl + F: Replace syntax in a script with another one (choose one by one if needed).

    • Shift + Ctrl + R: Replace all syntaxes in a script at once.

    • Ctrl + Space: Auto-detect code and suggest commands. Write the first letter of a command, then select the correct one from the list.

  3. Main features in the script editor:

    • Helpers: Predefined code snippets (e.g., if-then statements).

      • Loops and iterators: Includes Array, Repeat…Until, and more.

      • Math: Random value, Ceiling, Absolute value, Round, etc.

      • Objects/KNX bus: Get object value, Group read, Group write, Update interval, etc.

      • Storage: Retrieve and save data.

      • Script control: Manage other scripts (enable/disable).

      • Alerts and logs: Create alerts, log variables, and formatted alerts.

      • Time functions: Delay script execution.

      • Miscellaneous: Sunrise/sunset, etc.

      • Serial: Communication through internal controller I/O ports.

      • Modbus: Create RTU/TCP connections, read/write registers.

    • Group addresses: Existing group addresses on the KNX bus.

    • Objects by name: Choose objects by name.

    • Tags: Select objects by tag.

    • Data types: Choose objects by data type.

    • Scripts: Lists of event-based, resident, scheduled, and startup (init) scripts.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?