250929_LSS100100/LSS100200_SW_03.0

Event Script

Clicking in the object list opens the script editor in the next tab of your browser, allowing you to create an event-based script. The script will run each time a telegram is sent to the selected group. If the script is attached to a group, the icon turns green .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?