250929_LSS100100/LSS100200_SW_03.0

Backup

To create a backup, follow these steps:

  1. Backup all data: This includes objects, trends, logs, scripts, icons, images, backgrounds, visualizations, and the KNX filter table. The backup will be saved as a file named Project-device name-dd.mm.yyyy-hh.mm.tar.gz. The date and time used in the filename will correspond to the actual time and date when the backup is generated on the controller.

  2. Choose a password: During the backup process, you will be prompted to select a password. This password will be required to access the contents of the backup file in the future.

  3. Locate your backup file: Once the backup process is complete, you can find the backup file in your browser’s Downloads folder.


Please note the following important points regarding the backup process:

  • Maximum backup size: The maximum allowable size for a backup file is 32 MB. After creating the backup, ensure to check its size. If the backup file exceeds 32 MB, you will not be able to restore it in the future.

  • Exclusions from backup: The backup process does not include system configuration, network settings, installed applications, passwords, or KNX settings. However, the KNX filter table is included in the backup.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?