250929_LSS100100/LSS100200_SW_03.0

Frame

The Frame tab allows you to display either internal or external webpages within the visualization. You can integrate Schedulers and Trend logs into the frame. To configure the Frame parameters, follow these steps:

  1. Source:

    • Choose from Scheduler, Trend log, or an external URL.

  2. Frame size:

    • Specify the desired width and height for the frame.

  3. Custom name:

    • Provide a title for the frame.

  4. Refresh interval (seconds):

    • Set the rate at which the frame content refreshes (maximum = 3,600 seconds).

  5. Persistent:

    • By default, frames load when the plan is visible and are removed when hidden (for performance reasons with many frames).

    • Persistent frames load during initialization and remain throughout (useful for apps like alerts).

  6. Hide in Smartphone:

    • When checked, the frame won’t be available in Smartphone visualization.

After defining the frame parameters, click the Add to plan button. A newly created object will appear on the map, which you can move to your desired location. Resize the frame by holding its edges.

Remember to adjust the element size and position (refer to Object).

Finally, click Save and reload plan to activate the frame.

NOTE: Some web pages may have JavaScript preventing frame usage. In such cases, the webpage will open in full screen rather than within the frame. For Schedulers or Trends, it is recommended to stretch the frame to maximum width (minimum width: 1024). The frame is visible only under PC/Tablet visualization. Ensure that Schedulers or Trends are not accessible from Smartphone visualization by adjusting settings in Vis. structure under a dedicated plan.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?