250929_LSS100100/LSS100200_SW_03.0

Trend Logs

Trend logs, also known as data logging, allow you to store selected data and compare different time periods from the past. Access the trend graphs and export data from the Start page under Trends.

If the Energy plugin is installed in your controller, an Energy section will automatically be created in Trend logs. This is where trend logs for each Energy plugin equipment are stored. You cannot view the details of read-only trends, nor can you edit or delete them. They are there to reload data in case of an internet outage. However, if the internet outage lasts longer than 12 hours, the data will be lost and cannot be reloaded.

Trend logs are stored in the internal SD card memory.

Avoid using trends visualization on smartphones.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.