250929_LSS100100/LSS100200_SW_03.0

Building Operation WorkStation

Schneider Electric’s EcoStruxure is a BACnet-certified Building Management System. The Building Operation WorkStation software is used to configure and commission the Enterprise Server and the Automation Server, enabling them to retrieve and send data to the controller.

For detailed information about the interoperability between the controller and Building Operation Workstation over BACnet, visit Schneider Electric website.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.