250929_LSS100100/LSS100200_SW_03.0

EnOcean → Interfaces

To connect a USB EnOcean gateway to your controller, follow these steps:

  1. Navigate to ConfiguratorEnOceanInterfaces in the controller interface.

  2. Connect your USB EnOcean gateway to the USB port on the controller.

  3. Click Rescan in the lower-left corner.

  4. Once the device is detected, it will appear in the list of interfaces.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?