5031NMML Key Input Unit
The field informations to configure SpaceLogic C-Bus 5031NMML Key Input Unit are described as below:
|
Applications |
This section displays the lighting applications. Up to two lighting applications can be defined and then used throughout the configuration of the 5031NMML Key Input Unit. By default, Lighting is selected in the Application 1 drop-down list and <unused> is selected in Application 2 drop-down list. To add Application:
Repeat the same for Application 2. NOTE: The Trigger and Enable options are available only in Application
2 drop-down list. It supports application addresses from 48 to
127, 202 and 203. The application selected in Application 1 drop-down list will not be listed in Application 2 drop-down
list and vice versa.
|
|||
|
Configuration |
Click Edit Device. The Edit Device dialog box appears. For more information, refer Edit Device. |
|||
|
Global Provides a set of functions for controlling the timing, learn mode, and infrared settings. |
Timing Parameters Provides the ability to control how key input will behave by human touch. |
Debounce |
By default, it is set to 48 ms. You can select a different debounce time from the Debounce drop-down list. When you press an input key, the mechanical action may cause contact bounce, which can result in multiple rapid signals. To ensure reliable switching, the unit waits for a preset time period before responding to the key press. This delay is known as the debounce time. |
|
|
Long Press |
A key input unit senses whether you press a key briefly or hold it for a longer duration. The Long Press setting defines the minimum time the key must be held for the unit to interpret the action as a long press. By default, the Long Press time is set to 400 ms minimum value of 96 ms. You can select the desired minimum duration (in milliseconds) from the Long Press drop-down list to define a long press event |
|||
|
Ramp 1 |
Ramp 1 rate can be set from instant to max 1020 seconds. By default, it is set to 4 seconds. It specifies the time taken to ramp a light from minimum to maximum brightness (or vice versa). |
|||
|
Ramp 2 |
Ramp 2 rate can be set from instant to max 1020 seconds. By default, it is set to 12 seconds. |
|||
|
Status Report Wired C-Bus uses a status reporting system (known as an message synchronisation or MMI), which provides automatic detection and correction of discrepancies between the states of grouped inputs and outputs. This status reporting occurs at periodic intervals. Increasing the frequency of status reporting decreases the response time in which errors are corrected. However, it increases the amount of network communication traffic. If different status report values exist in the same network, the smallest value is used. The Status Report drop down list allows the selection of the status report value. |
Allows to set the duration in mm:ss. Provides automatic detection and correction of discrepancies between the states of grouped inputs and outputs. By default, it is set to 3 seconds. Mouse over on the Status Report info icon to view the tooltip message. |
|||
|
Device Scenes |
Click Scene Manager. For more information, refer Scene Manager. |
|||
|
Learn Mode You can configure the unit for learn mode. |
Allow Learn Mode |
Only if you select the Allow Learn Mode check box, the Application Learn drop-down list will be enabled. By default, the Allow Learn Mode check box is selected. |
||
|
Application Learn |
Select the required option from the Application Learn drop-down list. The options are Current and Any. To determine whether learn mode can be used to group channels with other units of the same application address, select Current. To determine whether learn mode can be used to group channels with other units of any application address, select Any. |
|||
|
Unit Has Learned |
By default, it is set as No. When the Unit Has Learned check box is enabled, it indicates that the unit has been involved in a learn mode operation. |
|||
|
Disable All Keys Provides the ability to disable all keys remotely by defining an Enable Control group. |
Group The Enable Control group parameter is used to enable or disable the unit input keys. The Group drop down list allows selection of the Enable Control group. |
To add Group:
|
||
|
Disables When |
It determines whether the Enable Control group enables or disables the input keys when the group itself is enabled. For example, if the Enable Control group is enabled, and Disables when radio button is set to ON, then the input keys will be deactivated. |
|||
|
Unit Identification |
Unit Type |
Displays the unit type of the device. |
|
|
Catalogue Number |
Displays the catalog number related to the unit type. |
||
|
Firmware Version |
Displays the version number of the C-Bus interface firmware which exists on the physical network or which has been assigned to a logical representation of the unit in the database. |
||
|
Part Name |
Displays the part name which is stored in the unit hardware, that can be modified. You can edit the Part Name. Use numbers, alphabets, and special characters (!@#$%^&*()_+];[) up to 8 Characters. Convert all characters to uppercase. |
||
|
Unit Address |
Displays the address which is automatically assigned when the device is added. |
||
|
Serial Number |
Displays the serial number which exists on the physical unit.
|
||
|
Tag Name |
Displays the name that user can give to the logical representation of the unit. This name can be up to 32 characters long and is stored in the project database only. By default it is NEWUNIT. |
||
|
Notes |
Contains a location to add notes about the unit which is stored in the project database only. Use maximum character length of 255 and only numbers, alphabets and special characters (!@#$%^&*()_+];[). |
||
|
Status Status will be displayed only when the network is opened. |
C-Bus Voltage (V) |
Displays the device’s C-Bus network voltage value. Values are displayed only when the C-Bus network is open. |
|
|
Learn Mode Active |
Displays Yes when it is active on the device/network and displays No when it is not active. To refresh device status, right-click on Status section and click Refresh Status. |
||
Once configurations are completed, click Save to save the changes.