Software Version 2.14.0

Edit Device 5031NMML

  1. Select KEYE1 in the Devices in Project section.

    Once you select KEYE1, KEYE2, and KEYE3, an Information pop-up is displayed. You can connect up to four keys to the device.

  2. Click OK to proceed.

  3. Click Edit Device in the Configuration section of PROPERTIES.

    The Edit Device — KEYE1 dialog box appears.

    The below configurations can be performed in the Advanced Configuration  :

Keys

This 30M series Key Input Unit has one physical input key, three unconnected input keys and four virtual (scenes only) input keys.


Physical input keys

The physical input key permit input events which originate from the local key input unit or from a remote source. You can program the input key to control electrical loads using a Lighting compatible group or a C-Bus scene.

When a building occupant turns on a switch or adjusts a dimmer, the input key transmits a group or scene command over the C-Bus network. This command includes the macro function that you previously configured in the unit configuration dialog box.


Unconnected input keys

The unconnected input key is a virtual input key within a 30M series Key Input Unit. The unconnected input key remains an unconnected input key as long as the unit is not connected to a physical key element. The 30M series Key Input Unit series are modular Key Input Units which can be configured physically to have from one to four keys.

The unconnected input key can be programmed to control electrical loads remotely using a C-Bus scene. When the unconnected input key is connected to a 30M series Key Input Unit element, the input key changes to become a physical input key.


Virtual (Scenes Only) input keys

The virtual (scenes only) input key permits input events which originate only from a remote source. You can program the virtual input key to control electrical loads using remote C-Bus scenes only.

When a building occupant turns on a switch, the input key transmits a Trigger Group level across the C-Bus network to activate a C-Bus scene. The transmitted command includes the macro function that you previously configured in the unit configuration dialog box.


  1. By default, Keys tab is displayed.

    The Key 1, Unconnected Key 2, Unconnected Key 3, Unconnected Key 4, Virtual Key 5, Virtual Key 6, Virtual Key 7, and Virtual Key 8 section appears.

    NOTE: The keys highlighted in blue, is to indicate that it is an unconnected key. You can commission an unconnected key in the same way as a connected key.
  2. Refer the below table for configurations in Key 1 section:

    Function

    Select the required option from the Function drop-down list.

    When you select On, Off On Up, Off Down, Dimmer Up, Dimmer Down, Soft Up, Soft Down, Shutter Toggle, Shutter Open Toggle, Shutter Close Toggle, Shutter Open, Shutter Close, Bellpress and Shutter Stop, the Expiry Time and Expiry Function fields are automatically hidden, as these options do not use expiry settings.

    • If you select On, On Up, Dimmer Up, Soft Up, Shutter open Toggle, Shutter Open a confirmation pop-up appears and prompts you to apply the complementary function to the paired key. (Example: If one key is On, the other should be Off)

      • Click Yes to proceed and No to cancel the operation.

    • If you select any other shutter function combination, a warning pop-up appears.

    • If you select Preset 1, the below fields appear.

      • In the Level field, either drag the slider to set the value or select a level from the drop-down list.

    • If you select Timer, the below fields will appear.

      • Select the Timer Type.

    • If you select Scene or Fan Speed Cycle, the below fields will appear.

      NOTE: The Fan Speed Cycle and Scene functions will not be listed in the Function drop-down list if the Application Index for the Key is set to Application 2.
      • Select Scene 1 from Scene drop-down list when no Scenes are assigned in the device.

      • Select Scene 3 when Scene 1 and Scene 2 are already assigned to other keys.

      • You can edit and add a new trigger group to the application.

        NOTE: The Trigger Group address field lists the available trigger groups in the selected Application.
      • To add/edit the Trigger Group refer Group.
      • You can edit and add a new action selector to the application.

        NOTE: The Action Selector field lists the available action selector in the selected Application.
      • Select the value from the Ramp Rate drop-down list.

      • Click next to the Scene drop-down list. The Scene Manager window appears. For more information, refer Scene Manager.

    <Scene Modify> Function

    • If you select <Scene Modify>, the below drop-down list will appear.

      NOTE: The Scene Modify option is not listed in the Function drop-down list if the application index for the Key is set to 2 in application index drop-down list in Group field.
      • Select the required option from the Scene Modifying Key Function drop-down list.

      • When you select Timer function in Scene Modifying Key Function drop-down list, is displayed. Click >Define a Scene Modifying Key window appears.

      • If you have not commissioned any Scenes or Fan Speed Cycle functions for Keys or Virtual Keys the table appears empty.

      • If you have commissioned any Scenes or Fan Speed Cycle functions for Keys or Virtual Keys, the below table appears.

      • The key number is non-editable in Key column.

      • The Scene column displays the Scene (or) Linked Scene label for each key. The Scene (or) Linked Scene label is non-editable.

        The Recall 1 (%) / Recall 2 (%)columns for each Key is set to 100.

        • You can update the Recall 1 (%) / Recall 2 (%) value for each Key.

      • You can update the time in Timer column. It ranges from 0 to 18 hours 12 minutes 14 seconds.

        • You can increase or decrease the hours and minutes by increment of 1.

        • You can increase or decrease the seconds by increment of 5.

      • Select the required option from the Expiry column

        .
    • When you select Preset 1 function in Scene Modifying Key Function drop-down list, is displayed. Click > Define a Scene Modifying Key window appears.

      • The acceptance criteria 10 to 21 are applicable for Preset 1.

      • Recall 2 (%), Timer, and Expiry Function columns are disabled and non-editable.

    • When you select Preset 2 function in Scene Modifying Key Function drop-down list, is displayed. Click > Define a Scene Modifying Key window appears.

      • The acceptance criteria 22 to 24 are applicable for Preset 1.

      • Recall 1 (%), Timer, and Expiry Function columns are disabled and non-editable.

      • Click OK.

    • When you modify the Key, Scene, Recall 1 (%), Recall 2 (%), Timer, or Expiry Function, the changes are saved to the corresponding Block.

    • The changes made to the Key, Scene, Recall 1 (%), Recall 2 (%), Timer, or Expiry Function will be in sync across the functions Timer, Preset 1, Preset 2, and Scene Modifying Key Function > Timer, Preset 1, and Preset 2.

    • If you unassign a Scene or Fan Speed Cycle function from the Key, that Scene is not listed in the Define a Scene Modifying Key window.

    • If you assign/reassign a Scene or Fan Speed Cycle function to the Block, the previously saved values for Key, Scene, Recall 1 (%), Recall 2 (%), Timer, or Expiry Function is restored (not the default values).

    Group

    To add Group:

    • You can enter the name in Group field and press Enter in keyboard. The Group Name is created by taking the next available Group Address.

      The created Group is saved in the network.

      or,

    • Click . The Add Group pop-up appears.

    • Enter the required details and then click OK. The Group Name is created and listed in the Group drop-down.

      NOTE:
      • Use a unique application name for each network.

      • Enter a maximum of 32 characters for the Group Name

      • You can use numbers, letters and special characters excluding /,” and #.

    • Click Cancel to cancel the operation.

      To edit Group Name:

    • Click to modify the group name.

      NOTE: Edit button is disabled if the Group is set to <Unused>.
    • Make necessary changes and then click OK. You cannot edit the Group Address after it has been created.

    • When you select groups for an Application (1, 2) and update the Application Index, the inline Confirmation pop-up is displayed for each selected group.

      • Click OK to create the missing groups.

    Expiry Time

    Select the desired expiry time. Mouse over on the Expiry Time info icon to view the tooltip message.

    • When you set the expiry time to 00 H: 00 M: 00 S, and configure the Timer function, time validation error is indicated by a red border. Mouse over on the Expiry Time field to view the tool tip message.

    • If you click OK while an expiry time validation error exists for a Timer function, an Error pop-up is displayed.

      NOTE: The Expiry Time field ranges from 0 to 18 hours, 12 minutes, and 15 seconds.
    • When you select an occupancy function a Timer function:

      • Expiry Time is set to 00 H: 05 M: 00 S, and corresponding Block Timer 1 value is updated only if the timer was previously set to 00 H: 00 M: 00 S. Otherwise, the existing value is retained.

      • You can set the Expiry Time from 1 second to 18 hours, 12 minutes, and 15 seconds for timer functions. For non-occupancy functions, you can set the Expiry Time from 0 seconds to 18 hours, 12 minutes, and 15 seconds.

    Expiry Function

    Select the expiry function from the drop-down list.

    If you select Recall 1 / Recall 2, the below fields are displayed.

    • You can set a preset Level or select an existing Tag. The Level value ranges from 0–100% and 0–255.

      NOTE: The default Level is 100%, 255 for Preset 1 and 0%, 0 for Preset 2.
      • The percentage value increments by 1% (0–100%).

      • The level value increments by 1 (0–255).

      • You can update the Level by changing either the percentage or the level value.

        NOTE: When you change the percentage, the level updates. When you change the level, the percentage updates.
    • The Tag field lists the available Levels for the selected Group Address.

      • When you select a Tag, the Level field updates to the Tag’s Level.

      • When you select a Level that matches a saved Tag, the Tag field updates to the corresponding Tag.

      • You can edit an existing Tag or add a new Tag to the Group Address.

      • The Add Tag option is enabled only when a Group Address is assigned to the Virtual Key.

    • To add Tag:
      • You can enter the name in Level Name field and press Enter in keyboard. The Level Name is created by taking the next available Level Address.

        The created Level is saved in the network.

        or,

      • Click . The Add Level pop-up appears.

      • Enter the required details and then click OK. The Level Name is created and listed in the Tag drop-down list.

        NOTE:
        • Use a unique application name for each network.

        • Enter a maximum of 32 characters for the Level Name

        • You can use numbers, letters and special characters excluding /,” and #.

      • Click Cancel to cancel the operation.

        To edit Level Name:

      • Click to modify the Level Name.

        NOTE: Edit button is disabled if the Tag is set to <Unused>.
      • Make necessary changes and then click OK. You cannot edit the Level Address after it has been created.

    Repeat the step 2 for the configurations in Unconnected Key 2, Unconnected Key 3 and Unconnected Key 4 sections.

  3. In the Virtual Key 5 section, select the required option from the Function drop-down list. The options are <Fan Speed Cycle> and <Scene>.

    NOTE: The Fan Speed Cycle and Scene functions will not be listed in the Function drop-down list if the Application Index for the key is set to Application 2.
    • Select Scene 1 from Linked Scene/Scene drop-down list when no Scenes are assigned in the device.

    • Select Scene 3 when Scene 1 and Scene 2 are already assigned to other keys.

    • You can edit and add a new trigger group to the application.

      NOTE: The Trigger Group address field lists the available trigger groups in the selected Application.
      • Mouse over on the Trigger Group info icon to view the tooltip.

    • To add/edit the Trigger Group refer Group.
    • You can edit and add a new action selector to the application.

      NOTE: The Action Selector field lists the available action selector in the selected Application.
    • Select the value from the Ramp Rate drop-down list.

    • Click next to the Scene drop-down list. The Scene Manager window appears. For more information, refer Scene Manager.

  4. Repeat the step 3 for the configurations in Virtual Keys 6, Virtual Keys 7 and Virtual Keys 8 sections.

  5. Once configuration is done, click OK to save the configurations.

  6. If you click Cancel or Exit icon without saving the configuration, a confirmation pop-up appears.

  7. Click Yes to save the configuration and click No to cancel the confirmation pop-up.

Key Functions

The Key Functions tab provides advanced setup for each input key.

Micro Function

Action

Short Press

when you first press the input key after the debounce time.

Short release

when you release the input key before the long-press time is reached.

Long press

when you press and hold the input key longer than the long-press time.

Long release

when you release the input key after a long press.

NOTE: Each of these events corresponds to a micro function. A micro function may or may not generate C-Bus messages, depending on the micro function and the current state of the group addresses. Wired macro functions support a wide range of messaging capabilities.
  1. Click Key Functions tab.

    Key Functions section appears.

  2. You can update the Micro Function combination.

  3. Refer the below table for default Micro Function mapping.

    Function

    Short Press

    Short Release

    Long Press

    Long Release

    Unused

    Idle

    Idle

    Idle

    Idle

    On

    On Key

    Idle

    Idle

    Idle

    Off

    Off Key

    Idle

    Idle

    Idle

    On/Off

    Toggle

    Idle

    Idle

    Idle

    Dimmer

    Idle

    Toggle

    Downcycle

    End Ramp

    On Up

    Idle

    Mem Toggle2

    Up Key

    End Ramp

    Off Down

    Idle

    Mem Toggle2

    Down Key

    End Ramp

    Timer

    Toggle

    Retrigger Timer

    Idle

    Retrigger Timer

    Bell Press

    On Key

    Off Key

    Idle

    Off Key

    Dimmer Up

    Idle

    On Key

    Up Key

    End Ramp

    Dimmer Down

    Idle

    Off Key

    Down Key

    End Ramp

    Soft Up

    Idle

    Ramp Recall 1

    Up Key

    End Ramp

    Soft Down

    Idle

    Ramp Off

    Down Key

    End Ramp

    Preset 1

    Idle

    Recall 1

    Ramp Off

    Idle

    Preset 2

    Idle

    Recall 2

    Ramp Off

    Idle

    Shutter Toggle

    Recall 1

    Idle

    Idle

    Idle

    Shutter Open Toggle

    Recall 1

    Idle

    Idle

    Idle

    Shutter Close Toggle

    Recall 2

    Idle

    Idle

    Idle

    Shutter Open

    Recall 1

    Idle

    Idle

    Idle

    Shutter Close

    Ramp Off

    Idle

    Idle

    Idle

    Shutter Stop

    Recall 2

    Idle

    Idle

    Idle

    Fan Speed Cycle

    Scene

    Scene

    Scene

    Scene

    Scene

    Scene

    Scene

    Scene

    Scene

    Scene Modify

    Idle

    Toggle

    Downcycle

    End Ramp

    Custom

    Idle

    Idle

    Idle

    Idle

    NOTE: The Fan Speed Cycle, Scene Modify and Scene micro-function combinations are read-only and non-editable.
  4. If you update the Micro Function combination, the respective Key Function is updated accordingly on Keys tab vice versa (except for Custom).

    The Custom function is excluded from this automatic synchronization.

  5. If you select any micro-function combination other than the default values listed in the table, the Key Function is automatically set to Custom.

Corridor Linking

Corridor linking with sensors is an effective solution for office environments. It allows employees to arrive and leave without manually switching multiple lights on or off.

Example: When employees arrive at the office in the morning, they walk through the corridor and trigger an occupancy sensor, which turns on the corridor lights. As they enter their office, the multi-sensor detects occupancy and switches on the office lights. Once the office lights are on, the corridor linking function keeps the corridor lights on.

When the last employee leave the building, they turn off the office lights. This action triggers a lighting sequence that keeps the corridor lights on, allowing them to walk safely down the corridor and exit the building. After a configured delay, the corridor lights automatically turn off.

  1. In Corridor Linking section, select the Enable Corridor Linking check box.

    NOTE: Only if you select the Enable Corridor Linking check box, other all drop-down lists will be enabled.
  2. In Link Group drop-down list, select the required group address.

    • Mouse over on the Application drop-down list to view the tool tip message.

    • Mouse over on the Link Group info icon to view the tool tip message.

    • The Link Group drop-down list displays all available groups within the selected application.

    • You can add and edit Groups. For more information, refer Group.

    NOTE:
    • The selection of a Group Address is optional when selecting a Corridor Block or Office Block.

    • Group addresses assigned in Corridor Block and Office Block are reflected in group address in Block Assignments in Blocks tab and vice-versa.

    • When you select a Group Address, the Function is automatically set to On/Off. This applies only the first time you make a selection, when both the Group Address and Function are set to Unused.

  3. In Corridor Block drop-down list, select the corridor block. Mouse over on the Corridor Block info icon to view the tooltip message.

  4. In Expiry Time drop-down list, select the desired expiry time.

    NOTE: The Expiry Time field ranges from 0 to 18 hours, 12 minutes, and 15 seconds.
    • You can increase or decrease the hours and minutes by increment of 1.

    • You can increase or decrease the seconds by increment of 5.

    • You can also input a value manually to hours, minutes, and seconds.

    • Mouse over on the Expiry Time info icon to view the tooltip message.

    • Expiry Time set in Corridor Block and Office Block are reflected in Expiry Time in Timer section in Blocks tab and vice-versa.

    • When you set the Expiry Time to 00 H: 00 M: 00 S, time validation error is indicated by a red border. Mouse over on the Expiry Time field to view the tool tip message.

    • If you click OK while an expiry time validation error exists for a Timer function, an Error pop-up is displayed.

  5. In Expiry Function drop-down list, select the required option.

    NOTE:

    Expiry Function set in Corridor Block and Office Block are reflected in Expiry in Timer in Blocks tab and vice-versa.

  6. In Office Block drop-down list, select the required option. You can select same (or) different blocks for Corridor Block and Office Block.

    • Mouse over on the Office Block info icon to view the tooltip message.

    • For more information on Expiry Time and Expiry Function, refer step 4 and 5.

Blocks

The Blocks table displays the operating configuration of the key input portion of the unit. Each row in the table allows a Lighting compatible group to be associated with one or more input keys. It is here that the recall levels, timer value and expiry key function are specified. LED indicator assignments are also specified in the Blocks tab.

  1. In Block Assignments section:

    • Select the application index from the Application Index drop-down list. By default, the application index for Blocks 1–8 is set to Application 1.

    • Select the group address from the Group drop-down list based on the selected Application. By default, the group for Blocks 1–8 is set to <Unused>.

    • Once you update the Application Index or Group Address, the Key 1 to 4 and Virtual Keys 5–8 group addresses are updated, and vice versa.

      NOTE: Block Assignments, Keys Using the Block, and LED Assignment are disabled when a Scene or Fan Speed Cycle function is assigned to a Key or Virtual Key.

      Block Assignments, Recall Lvls (%), Timer, Keys Using the Block, and LED Assignment are disabled when Scene Modify function is assigned to the Key.

  2. In Recall Lvls section:

    • Select the recall value from Recall 1 drop-down list. By default, the Recall 1 value for Blocks 1–8 is set to 100.

    • Select the recall value from Recall 2 drop-down list. By default, the Recall 2 value for Blocks 1–8 is set to 0.

    • Any changes made to Recall 1 and Recall 2 are saved to the corresponding Block and reflected under the associated Key(s).

    • Changes to Recall 1 and Recall 2 remain synchronized across Functions (Preset 1 and Preset 2, and Scene Modifying Key Function > Timer, Preset 1, and Preset 2), Blocks, and vice versa.

  3. In Timer section:

    • You can increase or decrease the hours and minutes in increments of 1 in Timer 1 field.

    • You can increase or decrease the seconds in increments of 5 in Timer 1 field.

    • You can manually enter values for hours, minutes, and seconds. By default, the Timer 1 value for Blocks 1–8 is set to 00 h : 05 m : 00 s.

    • Select the required option from the Expiry drop-down list. By default, the Expiry value for Blocks 1–8 is set to Off Key.

    • Changes to the Timer or Expiry drop-down list are saved to the corresponding Block and reflected under the associated Key(s).

    • Changes to the Timer and Expiry settings remain synchronized with the Functions (Timer and Scene Modifying Key Function > Timer, Preset 1, and Preset 2), Blocks, and vice versa.

    • When the Timer 1 value of Blocks is less than 1 minute and you select that block as a Corridor Block and/or Office Block:

      • The Expiry Time under Corridor Block and Office Block in the Corridor Linking tab is set to 00 h : 05 m : 00 s.

      • The corresponding Block Timer 1 value is also set to 00 h : 05 m : 00 s.

    • Example: If you assign Block 3 as a Corridor Block and Block 4 as an Office Block:

      • The Expiry Time for both Corridor Block and Office Block is set to 00 h : 05 m : 00 s.

      • The Timer 1 values for Block 3 and Block 4 are set to 00 h : 05 m : 00 s.

    • When you set the Timer 1 value in the Blocks tab to less than 1 minute and configure the block as either a Corridor Block or an Office Block, the Timer 1 value automatically resets to 00 h : 01 m : 00 s.

  4. In Keys Using the Block section:

    • The following keys will be selected by default with Block and Key combination.

    • The Virtual Key 5 to 8 are listed as V5, V6, V7, V8 and displayed in orange colour.

    • If you do not assign a Block to a Key or Virtual Key, the Key Group Address on the Keys tab is set to Unassigned and Function to Unused.

    • If no Block is assigned to a Key or Virtual Key (Key Group set to Unassigned, and Function is set to Unused), you can assign only Scene, Fan Speed Cycle, and Scene Modify functions.

    • If you assign multiple Blocks to Key or a Virtual Key, the Key Group Address on the Keys tab is set to <Multiple>.

    • If you select multiple keys or virtual keys for a Block, the Block properties apply to all selected Keys.

    • If a Key with Timer, Preset 1, or Preset 2 functions assigned has multiple Blocks allocated, the additional properties of Virtual Key on the Keys tab are disabled.

    • After assigning multiple Blocks to a Key or Virtual Key, if you update the Key to a single group address on the Keys tab, only the Block with the selected group address remains checked, and all other Blocks are unchecked.

  5. In LED Assignment section:

    • You can select any one of the Block 1 – 8 for each Key. By default, Block 2 is selected for LED Assignment.

  6. In Indicator Brightness section:

    • Select the required option from the Indicator Brightness drop-down list.

    • The Indicator Brightness is set according to the selected Block, and vice versa.

Scenes

Scenes enhance the ability to control lighting and other electrical devices. You can create up to eight scenes and associate the scene with a key on the input unit. Each scene can have up to 10 commands included. A scene command is composed of a Lighting type group selection and a defined power level in percent.


The Scenes tab provides a view of the scenes which have been previously developed. Each programmed scene will appear as a column in the Scenes/Command table. If Scene 1 has been programmed, then each associated command will appear.

  1. Click Scene Manager. For more information, refer Scenes.

Scene Manager

  1. For more information, refer Scene Manager.

Indicators

The Indicators tab controls the behaviour of the input key LED indicator.

  1. In Indicator Brightness section, select the required radio button option. Refer the below table for option description.

    Options

    Description

    Fixed Level

    The Fixed Level radio button controls the LED indicators. When selected, the LED brightness is set according to the value specified on the Fixed Level slider located to the right of the radio button.

    Brightness is represented as a percentage between 1 and 100% .

    Setting the value to 0% turns the LED indicators off.

    The Fixed Level setting applies only when the associated Lighting type group (address) is ON.

    Level of Group

    The Level of Group radio button sets the LED brightness to follow the level of a specified Lighting type group.

    Level of First Block

    The Level of First Block radio button affects all LED indicators. The brightness follows the level of the Lighting type group.

    • By default, Fixed Level will be selected. The fixed level value is set to 100 % on the slider and 255 in the level drop-down list.

    • When you change the slider, the level drop-down list is updated.

    • When you change the level drop-down list, the slider is updated.

    • The percentage value increments by 1% (0–100%).

    • The level value increments by 1 (0–255).

    • Select the group address from the Level of Group drop-down list. For more information, refer Group.

      NOTE: When you select a Group Address, the Function is set to On/Off. Its applicable to the first time selection when both Group Address and Function are set to Unused.
    • The application index is set to Application 1 and is disabled for selection. Mouse over on the application index, to view the tooltip message.

    • Select the Level of First Block radio button option to apply its effect to all LED indicators.

  2. In Indicator Options section, select the Enable Timer Flash check box to enable LED indicator flashing when a timer is active on the key input unit.

  3. In Indicator Assignment section, select the required option from the table’s drop-down list to define how each LED behaves when the key function is active or inactive.

    Refer the below table for LED (1–4) style configuration:

    Style

    On Color

    Off Color

    Status (On)

    Orange

    None (disabled for selection)

    Always Off

    None (disabled for selection)

    None (disabled for selection)

    Always On

    Orange / Blue (based on your earlier selection)

    None (disabled for selection)

    Status (Dual)

    Orange

    Blue (read-only; changing the On colour automatically sets the complementary Off colour)

    NOTE: The Style options controls how the LED indicators operate.
    • Always Off — When you select this option, the LED indicators are turned off.

    • Always On — When you select this option, the LED indicators are always on.

    • Status (On) — When you select this option, a specified LED indicator will light when the button is pressed.

  4. In the Key Press Activity section, by default the Active check box is selected. If you uncheck the Active check box, the Set Brightness To slider and For drop-down list are disabled.

    • Key Press Activity section controls the lighting behaviour of the LED indicator.

    • Drag the Set Brightness To slider bar to determine the light level on a percentage basis when a key is pressed.

    • Select the seconds from the For drop-down list.

  5. Select the Enable Night Light check box to enable the Nightlight Color options and Ignore First key Press check box.

    • Enable Night Light check box is used to enable the LED to be lit continuously.

    • Select any one of the Nightlight Colour options (Orange or Blue) to control the behaviour of LED indicator at night time.

    • Select the Ignore First Key Press check box to stop the LED key indicator brightness from increasing when the key is pressed.

Power Failure

The Power Failure tab allows you to set the level that each channel defaults to when recovering from a power failure. The Power Up Levels after C-Bus Power Failure section contains options for restoring levels when the unit is recovering from C-Bus power loss. The recovery options only apply to Lighting compatible groups that are associated with programming blocks.

  1. In Power Up Levels after C-Bus Power Failure section, select the required radio button option. Refer the below table for option description.

    Options

    Description

    Restore to Previous Levels

    When you select Restore to Previous Levels radio button, each Lighting compatible group will be restored to the level it was at when the power failure occurred.

    Restore to Preset Levels

    When you select Restore to Preset Levels radio button, the values selected on the sliders will be used as the restore level.

    NOTE: Each row in Restore to Preset Levels table is equalling to a block.
  2. In the Restore to Preset Levels table:

    • Group column displays the name of the group address assigned to the block.

    • In the Level column, either drag the slider to set the value or select a level from the drop-down list.

    • When you adjust the slider, the level value updates automatically. When you change the level value, the slider position updates accordingly.

      • The percentage value increments by 1% (0–100%).

      • The level value increments by 1 (0–255).

  3. Select the Synchronise Sliders check box to adjust all sliders to the same level simultaneously.

  4. Adjust any Level slider when Synchronise Sliders check box is selected, so that all Level sliders automatically realign to match the position of the slider you moved.

  5. If you select Restore to Previous Levels option, Group, Level, and Synchronise Sliders options are disabled.

  6. Once configuration is done, click OK to save the configurations.

  7. If you click Cancel or Exit icon without saving the configuration, a confirmation pop-up appears.

  8. Click Yes to save the configuration and click No to cancel the confirmation pop-up.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.