Software Version 2.14.0

SENPIROA (5750WPL)

The SpaceLogic C-Bus 5750WPL is a high-performance outdoor Passive Infrared (PIR) movement sensor designed for the C-Bus automation network. You can use this sensor for security and energy-efficient lighting control in areas such as driveways, carports, and gardens. With an IP66 rating, it reliably operates in harsh outdoor weather conditions.


To configure the field informations of PROPERTIES in SpaceLogic C-Bus SENPIROA sensor, refer SENPIRIA (5751L).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.