Software Version 2.14.0

5041NMML Key Input Unit

The SpaceLogic C-Bus 5041NMML is a 40 series master push button mechanism designed for use in C-Bus automation systems. It functions as a Key Input Unit and provides fully programmable, intelligent control of lighting, dimming, shutters, and scene operations. The unit integrates seamlessly into iconic or pro series wall plates, delivering flexible and reliable user control within C-Bus installations.


To configure the field informations of PROPERTIES in 5041NMML Key Input Unit, refer 5031NMML Key Input Unit.

  • Click Edit Device in the Configuration section of PROPERTIES.

    The Edit Device — KEYE1 dialog box appears.

  • For more information on configurations in the Edit Device, refer Edit Device 5031NMML.

  • The key difference between the 5031NMML and 5041NMML models lies in the colour of Nightlight Options in Indicators tab.

    • 5031NMML : Orange and Blue

    • 5041NMML : Red and Blue

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.