Software Version 2.14.0

Introduction to Sensors

The SLCC tool supports a range of C-Bus occupancy and light level sensors designed for use in commercial and residential environments. These sensors provide reliable presence and occupancy detection, light level measurement, and advanced control features such as corridor linking, sunset switching, and breakout room functionality, depending on the model. Available in flush mount and surface mount variants, the supported sensors offer different detection patterns, mounting options, and coverage ranges to suit various installation requirements. Through the SLCC tool, you can configure sensor behavior, assign groups and blocks, and integrate the devices seamlessly into C-Bus lighting and automation systems.

Refer the below table:

Sensor

Image

5753L (SENPIRIB)

5754ODPE (SENPIRIC)

5751L (SENPIRIA)

5750WPL (SENPIROA)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.