Software Version 2.14.0

DALI 2 Gateway Conversion

If there are old Gateways existing in the project, the SpaceLogic C-Bus Commission allows you to convert old Gateways to new DALI 2 Gateways.

List of old DALI 2 Gateways that can be converted to new DALI 2 Gateways.

Old Unit Type

New Unit Type

PC_DAL2B

SYS_DAL2

PC_DAL2C

SYS_DAL2

To convert:

  1. Open the same project in commission software same as in Toolkit where the device (old Gateway) is added in network.

  2. Select C-Bus Devices of the network.

    The available devices in the project are displayed.

  3. Select the device (old Gateway) that needs to be converted.

  4. Right click on the Gateway > Convert Unit.

    Convert Unit pop-up is displayed.

  5. Click OK.

  6. The old Gateway is converted to new SYS_DAL2 — C-Bus DALI-2 Gateway.

IMPORTANT: When conversion is completed:
  • The address of the Gateway remains the same.

  • The unit type catalogue description and firmware details are updated.

  • The firmware will have the latest version.

  • The serial details needs to be updated manually in property window of the device.

  • The configuration changes made in old Gateway reflects in the new Gateway as well.

    Table below shows the list of properties that will be restored in the new Gateway.

    List of properties that will be restored in the Gateway, and SYS_DAL2

    Properties

    Properties which are restored

    Properties which are not restored

    Project Name

    Project name will be restored as in the existing Gateway

    Not Applicable

    Applications

    Applications will be restored as in the existing Gateway

    Not Applicable

    Global

    Enable C-Bus Clock

    Enable Burden

    C-Bus to DALI Map

    • C-Bus Group Address mapped to DALI Line A Broadcast

    • C-Bus Group Address mapped to DALI Line B Broadcast

    • C-Bus Group Address mapped to DALI Group

    • DALI to C-Bus Mapping

    • C-Bus Group Address mapped to DALI Off

    • C-Bus Group Address mapped to DALI Scenes 1 to 16

    The serial details needs to be updated manually in the property editor.

Once the conversion is completed:

  1. Scan the C-Bus network.

  2. Identify new relay on the Network.

  3. Readdress the device to match live network or readdress device to match the project database.

  4. Deploy the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.